Part Number: SN65C3232E
Hi team,
My customer provided a question in terms of capacitor value for SN65C3232E.
Datasheet shows VCC vs CAPACITOR VALUES table and it describes C1: 0.047µF/C2-C4 : 0.33 µF respectively under VCC=5 V ± 0.5 V.
The customer thinks these value are relatively large under condition that cable length is <1m and VCC=5V.
Would it be possible to reduce capacitor such as 0.1uF from 0.33uF under condition that cable length is <1m and VCC=5V.?
I'm looking forward to hearing back from you.
Best regards,
Shota Mago