Part Number: TUSB211
Other Parts Discussed in Thread: TUSB217
Hello
Below is customer topology. If remove re-driver 1 just reserve re-driver2 on board, the eye diagram are below and looks bad. Has any suggestion how to pass eye diagram testing? Thank you.
|
CPU-->PCIE connector |
9 inch |
|
PCIE connector-->re-driver1 |
2 inch |
|
re-driver1-->re-driver2 |
10 inch |
|
re-driver2-->USB switch |
8 inch |
|
USB switch-->USB port |
2 inch |
No re-driver
level0 120ohm
level 1 2kohm
level2 3.9kohm
level 3 7.5kohm
BR
Patrick