Part Number: DS90UB933-Q1
Other Parts Discussed in Thread: DS90UB954-Q1
Hi,
I trying to connect this 933 in the following configuration:
1. Mode setting : External oscillator mode using 48 Mhz crystal
2. Pclk is from Image Sensor is 96Mhz connected to PCLK of the 933
3, My sensor feed in to 933 is 8 bits instead of 10 Bits
Din 0 to Din 7,of 933 inputs connected to Data0 to Data7 of my sensor output
Din 8 to Din 11 of 933 input is connected to Gnd.
Does this work for the 933?
Thank You