Part Number: DP83822I
Hi Team,
Customers attach digital transistors to the LED_ 0 port for LED drive.
At startup, the voltage of LED_ 0 (Strap pin) becomes 1 V, serial communication is not performed.
If they do not connect a digital transistor to LED_ 0, make sure to communicate with the MAC.
· Can I add a digital transistor to LED_ 0, LED_ 1?
· What happens when the LED_0, LED_1 does not belong to the range of MODE 1 ~ 4, when the strap voltage is?
Best Regards,
Kenji