This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65987-90EVM: PSIL034C default pjt/bin files

Part Number: TPS65987-90EVM
Other Parts Discussed in Thread: TPS65987

Hello -

I have been trying to locate the default project file for the TPS65987-90EVM PSIL034C kit.  According to the users guide the board is configured out of the box as a DRP.  I would like to be able to make small changes to the configuration and then be able to roll back to a default configuration if I don't understand some behaviors.  

I have taken a snapshot of the default board in debug mode.  While I think I could use that to make a configuration it would be much less error prone to have the actual project file.  Additionally, I don't see any way to read the APP CONFIG DATA TABLE on the default board.  It appears that I2C1 is configured to talk to address 0x40.

Also is there a way to read the BIN file from the SPI flash?

Thank you,

Dave