Part Number: UA9637A
Hello,
I have a couple of questions about UA9637A termination.
1) Regarding the differential input, it looks that an external input termination has to be added, is it correct? If yes, is the right value 50ohm?
2) Regarding the single-ended output, it looks that it has 50ohm impedance at high level output. When the output has a long routing, should we add 50ohm termination on the load termination to prevent unexpected signal reflection?
Thanks in advance.
Shinya Sawamoto