This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65981: TPS65981 and TUSB8020 connection

Part Number: TPS65981
Other Parts Discussed in Thread: TUSB542

Hello,

 

I want to realize a board that can be connected to a tablet through type-C USB.

This board is UFP and Power source. Then I want to put TPS65981.

And I also want to put TUSB8020 to connect a USB2.0 device IC and USB3.0 connector.

Then I want to confirm whether the below connection make sense.

Does it make sense?

 

Regards,

Oba