Part Number: LMH1297
When designing my board using the LMH1297, what target impedance should I be using? Also what is the frequency range I should be targeting to stay under that impedance? Right now I was targeting 100mOhms as my target impedance. This based on a 66% dynamic current, 150mA operating current, 2.5V rail and 0.4% ripple. (0.4% ripple is based off the requirement of 10mVpk-pk supply ripple). Thanks.