Part Number: SN75DP159
Other Parts Discussed in Thread: TDP158
Hello,
In one of my early questions about swap functionality of DP159, I was told that the OUT_CLK pair PLL is limited to 340 MHz in retimer mode and that is why the swap feature of DP159 / DP181 is different than TDP158.
Related to the DisplayPort X-mode, if that OUT_CLK pair is limited to 340 MHz, can I have truly retimer functionality, ie enhanced eye diagram, directly from DP159 output (as for the case if my input signal is HDMI)? Or that retimer functionality is done indirectly through AUX_SCR pair, the FPGA would use that reference clock to clean up the eye diagram of the signal received from DP159?
Thanks
Lam Huynh