Part Number: THVD1510
Other Parts Discussed in Thread: THVD1500, , TVS1401
Hello all,
in the TVHD1510 datasheets (THVD15xx devices RS485 transceivers) as in other devices and application notes
a suggestion for single stage surge protection is by using the SM712 (Bourns).
My question is how the SM712 device can provide surge protection at 1KV (8/20usec) as defined in IEC 61000-4-5.
According to IEC 61000-4-5 the 1KV surge voltage will discharge through a resistor of 40+2 Ohm, producing a current of almost 24A (23.8A).
In the specs of SM712 (3 manufacturers) the max clamping current is lower than 24A,
and with some degradation due to temperature (assuming a working temperature of 50oC),
the clamping current is reduced to 80%.
| 25oC | 50oC | |
| Bourns | 17A | 13.6A |
| Littelfuse | 19A | 15.2A |
| Semtech | 21A | 16.8A |
So, it seems to me, that the above devices would not withstand the surge current.
In the case where we assume the bus lines as symmetrical lines, we could split the surge current with two 40 Ohm resistors,
which then would be (1000V/40R)/2 = 12.5A.
In this case the above devices would withstand the surge current,but
the clamping voltage will still be higher than the absolute maximum voltage on the bus pins (THVD15xx : +/- 18V)
| Neg. Pulse | Pos. Pulse | |
| Bourns | -13.1V | 23.8V |
| Littelfuse | -16V | 26V |
| Semtech | -11V | 21V |
(note: I am not fan of this approach, as in real industrial world the bus lines could be anything but symmetrical)
The above clamping voltages are extracted by the graphs in the data sheets (Semtech,Littelfuse),
and extrapolated (Bourns) by the data given. Neg. Pulse : (1A,11V),(1A,19V) and Pos. Pulse (1A,19V),(17A,26V).
The way I see it, in any case the bus pins on the transceivers are unprotected and the devices will be destroyed by the surge pulse.
The 10 Ohm series resistors will definitely limit the current flowing in the pins,
and the energy dissipated on the transceiver due to surge pulse, but there is no information in the data sheets regarding this.
Apparently so many wise engineers in TI and in the community now better,
but I am trying to understand the way the SM712 protect the transceivers and at the end how I can choose the proper TVS device.
Please enlighten me and comment at will.
TI Transceivers: THVD15xx
Bourns : SM712
Littelfuse : SM712
Semtech : SM712
PS : Having read a number of application notes, blog articles and datasheets, I have to thank all these TI engineers provide this knowledge.