Part Number: TUSB542
Other Parts Discussed in Thread: TUSB321,
Hi,
We plan use TUSB542 + TUSB321 for type C DRP 2:1 MUX. Would you help review if our schematics below ? thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
PYTsai,
Please see may notes below. Could you give more description of your application? With better explanation I can provide more detailed notes.
David,
1. The RX_AP and TX_AP are connected to our host ASIC on the board as below. And it follow the orientation.
As we know the USB3 interface supports pair swapped. Does the three USB 3.1 interfaces of TUSB542 support pair swapped ?
2. Yes we have a VBUS switch on the system. Should I connect ID of TUSB321 to notify MCU in order to turn-on the VBUS switch?
Thanks!