Part Number: SN65HVD234
1. There is no figure given in the datasheet for receiver input resistor matching.
2. There is no figure given in the datasheet for Driver symmetry.
Can those values be provided?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65HVD234
1. There is no figure given in the datasheet for receiver input resistor matching.
2. There is no figure given in the datasheet for Driver symmetry.
Can those values be provided?
Hi Eric,
The standard ISO11898-2 defines an driver symmetry of 0.9 - 1.1, from the formula vsym = (VCAN_H + VCAN_L)/VCC. Assuming the datasheet worstcase values for VCAN_H and VCAN_L i work this out as just outside the limits.
The standard also defines the receiver input resistance matching, the datasheet provides single ended and differential resistance, but i cant equate that to how the two resistors are matched. The ISO standard requires mR = -0.03 - 0.03, (mR = 2 × (RCAN_H − RCAN_L)/(RCAN_H + RCAN_L).
I wondered if you have specified values for these parameters.
Best Regards,
Dan