Part Number: SN65DSI85
Other Parts Discussed in Thread: DSI-TUNER
We have about ten prototype systems with the SN65DSI85 running. Occasionally on a few of them we lose displays. A power cycle will bring it back. Today we were able to catch a failure while we were all instrumented up and we saw that the error register 0xE5 was 0x35. Which says, PLL_UNLOCK, CHA_SOT_BIT_ERR (leader sequence bit error), and that it detected an uncorrectable and correctable error.
I was surprised to see PLL_UNLOCK because we are using a local oscillator at 74.25MHz. Is there some kind of DSI error that would also knock the PLL out of lock? We were able to get the part working again by just re-writing the configuration over I2C, but I'd like to get to the root of the problem too. Also the distance between our DSI source and the TI chip is 2-2.5". So it's a pretty short run, all matched impedance, matched length etc.
FInal question. Can we recover from this error or do we have to reset the TI part everytime?
Thank you,
-Eric