This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB913Q-Q1: DIN0-DIN11 connection method

Part Number: DS90UB913Q-Q1

Hello

Can i connect the image sensor IC's output data line with DIN0-DIN11 like this:

IMX291----->  913

CIS_D2----> DIN0

CIS_D3---> DIN1

...

...

...

CIS_D11--->DIN9

CIS_D0----->DIN10

CID_D1-----> DIN11


The 914's Rout are in the same sequence to connet with ISP IC.

Is there any problem about this circuit?