Part Number: TCAN4550-Q1
Hello Expert,
I'd like to use ECC self test by injecting an ECC error. The message RAM on TCAN45x is 2KB in total, what is the size of ECC memory area? How many ECC bits are used for 64-bit memory data?
In the test register (080C), I wrote 0x000000 to [21:16] to select bit 0 (same for bit 1?), and set bit 12 to force a single bit ECC error, then I read bit 11, but this bit is not set. How can use this feature? What do [31:24] (Test Read and Write register) and [23:22] (Test Read and Write) mean? and What value should I write to those bit field?Thanks for help