Part Number: TCA6416A
Other Parts Discussed in Thread: TCA6424, TCA8418E, TCA8418
Hi team,
My customer want to use TCA6416A for button detection. Below is the illustration diagram, actually they have 5*4 button. They want to use TCA6416A to save IO numbers.
1. Can I use TCA6416A to realize 5*4 button detection? I assume that totally 9 IOs of TCA6416A is uesd, once a button is pressed, TCA6416A send a Interrupt signal to MCU, and MCU check the register's status and calculate which button is pressed, then reset the register.
2. Usually we need anti-shake function when use GPIO and software to realize button detect. Software will delay several us to avoid multiply detection for one press.
3. Another option is use TCA6424, for each button, is this better for detect speed?
Thanks