Part Number: DS90UB964-Q1
Dear Sir,
I have a question:
four OV10640+OV490+DS913 connected to a DS964 , configured with DS964 in 4 channel framesync mode, and the synchronous signal is generated by DS964 internally generated framesync (GPIO0/GPIO1 outputs frame sync to sensor module). The CSI-2 forwarding mode is configured to best-effort round , the prototype is work;
But when the CSI-2 forwarding mode is configured to basic synchronized forwarding. there is no image output , The status register values are as follows:the red arer abnormal.
reg=0x35 val=0x0 successed!
reg=0x36 val=0x0 successed!
reg=0x37 val=0x3 successed!
reg=0x4d val=0xc3 successed!
reg=0x4e val=0x14 successed!
reg=0xda val=0x0 successed!
reg=0xdb val=0x10 successed!
reg=0x73 val=0x2 successed!
reg=0x74 val=0xd0 successed!
reg=0x75 val=0xa successed!
reg=0x76 val=0x0 successed!
reg=0xb9 val=0x3 successed!
i want to know the detail reason about this, thanks a lot.