Part Number: DP83822H
Hi,
My customer is planning to use the PHY for a new design. For the same I have some queries as follows:
- PHY to MAC communication through RMII is facilitated by the chip?
- For master mode & slave mode we need to provide 50 MHz & 25 MHz clks respectively. So, if we want to use the same module to be configurable to both modes, do we need to put two oscillators in switched manner? Kindly clarify.
- In RMII mode, TX_CLK & RX_CLK will be unused. At which pin Ref. CLK will be available to be routed to MAC.
Regards,
Aniket