Part Number: TUSB2046B
Tool/software: Linux
I have a problem with my HUB (TUSB2046B).
I would like to use the chip with an IMX6 processor and unfortunately
the system isn't working properly. The SUSPEND pin oscillates after starting the System between high and low therefore the host cannot communicate with the TUSB2046B-Chip.
I have three different circuit boards and for all three I have the same problem. The USB communication always interrupts (voltage at D0+ swings all the time) and I don't have a stable Oscillatorsignal from Crystal because the chip oscillates each time (active/rest mode). I changed the crystal oscillator and the values of the two capacitors from 27pF to 22pF and always had the same problem.
The same circuit has already been implemented and had good works. Now I do not understand why the system is unstable and not works.
Maybe someone here can help me?