This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1043-Q1: Automotive Single Wire CAN Transceiver Solution

Part Number: TCAN1043-Q1

Hi team,

Could you please help to check if we have single wire CAN transceiver solution, like NCV7356/TH8056?

Thanks!

  • Fery,

    Our CAN transceivers can work as a one-wire CAN interface if CANH is used as the output and CANL is shorted to ground while termination is in place. Looking at both datasheets for the NCV7356 and the TH8056, they are both compliant to GMW3089. If that is a requirement from the customer, we don't have any devices that support this compliance. A specific physical layer is used for transceivers compliant to GMW3089, and our transceivers are not designed to be compliant with this standard.

    What kind of application is this? Does the customer need the GMW3089 compliance?

    Regards,