This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB954-Q1: TI954 and TI953 case

Part Number: DS90UB954-Q1


Hi

We are use DS90UB954 and DS90UB953 serdes to connent  camera module and host. Basic data follow is 

Host->TI954->LVDS->TI953->IMX390. We want to use exteral GPIO from host to trigger IMX390 frame sync.

The trigger  GPIO0 from TI954 will be used as trigger pin. And TI953 GPIO3 is connected with IMX390 frame sync pin.

But we found pull/down GPIO0 can't trigger GPIO3 signal. Below is our setting, pls help review and give right register

config. Thanks

954:
0x4c, 0x01
0x21, 0x81
0x33, 0x23
0x20, 0x20
0x42, 0x71 
0x5c, 0x30  ---- SERDES address
0x5d, 0x42  ---- SENSOR address
0x65, 0x42  ---- SENSOR address
0x6e, 0x99
0x58, 0xde
0x6d, 0x44
0xd5, 0xf0
953:
0x02, 0x33