Part Number: TUSB8020B
I am looking for the programming tool for the TUSB8020B.
I would like to set the port removable configuration for downstream ports 1 and 2.
I assume this is a windows based tool, which I can run on an upstream connected PC.
Do the SCL/SDA pins need to be pulled up to program OTP (as per the datasheet)? No external interface is used on our product (no EEPROM, etc.), and so these pins are not connected to anything currently. Could potentially add TP's for programming this in a test jig if required.
Thanks,
Chris