Part Number: TMDS181RGZEVM
Other Parts Discussed in Thread: ESD224, SN65DP159, TMDS181, TPS62150A
Hi Support,
For TMDS181RGZEVM, noticed that there are no any ESD protection on the board, so according to our HDMI2.0 (IN/OUT) and TUSB3.1 (In/Out) connect board,
- Do the ESD need to protect ? such as ESD224 for HDMI2.0
- The ESD IC on the board would affect the Eye Diagram?
- So which should be better (ESD on board or not).
Thanks.