This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB522PEVM: ESD Queries

Genius 5355 points

Part Number: TUSB522PEVM
Other Parts Discussed in Thread: ESD224

Hi Support,

For TUSB522PEVM,  noticed that there are no any ESD protection on the board, so according to our TUSB3.1 (In/Out) connect board,

  1. Do the ESD need to protect ? such as ESD224 for USB3.0.
  2. The ESD IC on the board would affect the Eye Diagram?
  3. So which should be better (ESD on board or not).

Thanks.