Part Number: TPS65981
Hello,
I am building a USB type c connector based system but I cannot have the USB2.0 lanes go to the TPS65981. I also will be using alternate modes with extending displays and having a high speed USB pair for additional perhiperals.
I am struggling to understand if not having the TPS65981 USB 2.0 path has me giving up features of the device? It looks like it is an analog mux. I have the TPS65981EVM and I have 20V and the alternate modes working but was not sure if any USB2.0 data was exchanged in addition to CC,SBU.
Thanks for clarification,
Jason