Part Number: SN65HVD33
Hello support team,
I will ask about the driver enable time of SN65HVD33.
1. Can I understand the time from when the driver is enabled to when the output signal is output as follows?
Described in "Switching Characteristics: Driver" on page 11 of the datasheet,
"tPZH1: Propagation delay time, high-impedance to high-level output"
or "tPZL1: Propagation delay time, high-impedance to low-level output" of the data sheet "Switching Characteristics: Driver"
2. What is the difference between "tPZH1, tPZL1: Driver enable delay with bus voltage offset" in datasheet "Switching Characteristics: Driver" and the above 1?
3. Can I understand that Vo = 2 V (typ) of "tPZH1, tPZL1: Driver enable delay with bus voltage offset" is the same as when the common mode voltage is 2 V?
4. A graph of "Figure 15. Enable Time vs Common-Mode Voltage" is shown on page 14 of the datasheet. Looking at this, Enable Time is over 400 ns when the common mode voltage is 3.5 V or higher.
I think that this is a different result from the above 3.
How should I understand?
5. Our customer is using at 1.9 V of the common mode voltage. And about 430 ns of delay has occurred until X and Y are output after DE goes 'H'. I think that it differs from the above understanding. How can I understand about it?
6. Does the common mode voltage that increases Enable Time vary?
How much is the variation?
7. Do I need to consider the maximum value of "Driver enable delay with bus voltage offset" which is 900 ns in any usage conditions as driver enable time?
Sincerely,
M. Tachibana