Part Number: TUSB3210
Other Parts Discussed in Thread: TUSB3410
Hello,
I have a "usbclient.bin" file that is being downloaded to the TUSB3210 from a Linux host when the device is connected.
Please help me find a solution for how to do the same when the device is connected to a MacMini computer running MacOs.
The device containing the TUSB3210 is some kind of a USB-UART transceiver.
Should it be possible to use the same ".bin" file when using MacOs?
Side question: Do you think it would work if I simply write the "usbclient.bin" to an EEPROM using your TUSB3x10 EEPROM Burner?
Best Regards,
Eduard Andrasi