Part Number: TUSB2046B
I designed a PCB with the TUSB2046B 4 port Hub. when I plug in the board into a windows 10 computer I can see the USB hub as windows ca recognize the device. The issue I have is when I plug in a USB 3.1 Camera. I am getting a "Descriptor failed" and the device is not recognized by Windows 10.
When I plug in a USB 2.0 Camera into the HUB, windows 10 can recognize the camera and it works well.
I cannot get a USB 3.1 device to work with this IC. USB 3.1 is suppose to be backwards compatible so windows should be able to recognize the device. Is there an issue with the IC? Why cant I see the USB 3.1 Camera?
Thanks
Chris