Part Number: DS90CR287
Other Parts Discussed in Thread: DS90CR288A
Hi,
There is a question aboout DS90CR287&288A.
Our camera output interface is DVP, using 8bit Data, 1 vsync signal, 1HREF signal and 1 pclock. We want to use DS90CR287 to transform DVP interface to LVDS, and use DS90CR288A to transform LVDS to DVP.
I want to confirm that is there any connection order of these data signal? And is this need fixed data format?
I think this two ICs can transform any parallel data(need one clock signal) to 4lane LVDS signal. What we should do is make sure that the DS90CR287&288A have the same IO allocation.
Please help us to cofirm it.
Thanks!