DS90UB926QSQX/NOPB for image transmission application: when using 50 Ω coaxial cable as transmission medium always need two single core coaxial cable to transmit an LVDS signal, could you tell me whether you can use one of the single fiber coaxial cable on the signal transmission power, in order to reduce a single coaxial cable as MAX96705 Maxim.Wiring is as follows: