This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DPHY440SS: Which materials are available for wire ?

Part Number: SN65DPHY440SS

Dear  all

     For DAxP/N and DBxP/N to , Which materials of wires are available? 

  • Hi Went,

    DAxP/N and DBxP/N are 100-ohm differential impedance. Material could be either pcb trace or twisted pair cable. Please note SN65DPHY440 equalizer has either 2.5dB or 5dB gain at 750MHz. So pcb media or twisted pair cable insertion loss should be within this range.

    Regards,,nasser