Part Number: TPS65986
Other Parts Discussed in Thread: TPS65987D
Team,
Is there some proven/available flow that can be programmed in the TPS65986 to monitor an External Temp Sensor through a GPIO, and when it exceeds a threshold, cause either PD disconnect, or at least re-negotiation to PDO-0 (5V)?
Any direction you can provide is appreciated. I see that GPIO's can be routed to the ADC for Analog Voltage monitoring... or there is potential for a digital output "thermostat" device to provide just a high/low input signal, if that is easier to program/implement.
Thank you,
Eric.