Part Number: SN65DP159
Our firmware team observed that the DP159 LOCK_COMPLETE bit remains stuck at b1 after the input to DP159 (host/source) has been powered down or DP cable disconnected. LOCK_COMPLETE appears to be a one-shot latching status bit. Questions:
1. Is LOCK_COMPLETE a one-shot latching status bit ?
2. What register bit or logic condition causes LOCK_COMPLETE to reset to 0 ?
This behavior was observed and is of interest because our firmware team was interested in using DP159 PLL_CLOCK and/or LOCK_COMPLETE or other status from DP159 as means of detecting when host/source was powered-off but still connected to DP159 input.
The LOCK_COMPLETE stuck behavior was reported in another TI e2e thread but there is no final resolution or explanation:
https://e2e.ti.com/support/interface/f/138/t/512479?DP159-Digital-Lock-Detect-Output
Regards,
KT