Part Number: TUSB8041
Hi, could you please confirm below questions regarding the reset design for the hub.
1. The max allowed voltage on GRSTz for an active L is 0.8V? What if there is a period of time the voltage is 1V, is the hub in reset state or not?
2. I saw on the EVM board, the GRSTz pin is connected to a 1uF capacitor which means host will not be able to reset the hub via the GRSTz pin. We are wondering if the hub is malfunctional or lost connection to host(such as due to an ESD event), is there a mechanism able to detect this situation and do a warm reset ?