Part Number: TPS65987D
Hi Team,
My customer considers to use TPS65987D in his system.
The system is USB2.0 and provider (source only) application.
He wants to change source power dynamically depending on system state.
For example,
1) Consumer device is connected to the system (TPS65987D) through Type-C cable.
2) TPS65987D provides power to consumer device depending on PD communication (ex. 15V/3A).
3) CPU advertises TPS65987D to reduce power.
4) TPS65987D reduces power provoided to consumer device (ex. 15V/3A -> 5V/0.1A).
Is it possible scenario for TPS65987D?
If the answer is yes, how to achieve 3) process?
Is it required I2C communication between CPU and TPS65987D?
Best Regards,
Yaita