Part Number: TPS65987EVM
Other Parts Discussed in Thread: TPS65987
Hello!
I would like to use TPS65987EVM as a source to deliver 20V/max current (5A ?) via USB-C. It is clear how to configure the jumpers J6 and J4.
My question is about the variable DC-DC converter. I want to configure it to 20V output (or maybe to bypass it if possible?). To configure it to 20V output I
need to program 3 pins of the USB controller: PDO_1, PDO_2, PDO_3. I tried to use the Application Customization Tool to program them and I could not setup the
communication, so I need your support there. I used the USB cable for that and did not succeed to setup the communication.
Another question I have is what is the maximum output current the variable DC-DC converter can deliver @ 20V output.
Thanks and Regards,
Natasha