Part Number: DS90UH947-Q1
Hi Team,
If register 0x4F, bit 6 (OLDI_IN_MODE) is configured for dual-pixel mode and bit 5 (OLDI_IN_SWAP) is a value of 1, does that swap the bank of OLDI inputs (D0-D3) with the other bank of OLDI inputs (D4-47)? So, for example, the table below defines the processor output and the 947 input. Will the swap function from OLDI_IN_SWAP make the appropriate swap for the configuration below?
| Processor Output | 947 Input |
| D0 | D4 |
| D1 | D5 |
| D2 | D6 |
| D3 | D7 |
| D4 | D0 |
| D5 | D1 |
| D6 | D2 |
| D7 | D3 |
Thank you,
Jared