Part Number: TDP158
Working on getting a initial settings for all our registers for my company and saw that the TMDS clock ratio field was updated from DDC snoop on I2C that occurs on the source side of the interface. We haven't sent out the circuit board for fabrication yet but have the design referenced towards the application example shown in Figure 46 where the source side is always grounded. If we use the figure as a reference then it seems that the automatic termination would always have to be changed when we switch the rate from HDMI 1.4 to HDMI 2.0 or is the text in the register map incorrect and will see the DDC snoop on the sink side also to change the termination?