This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB935-Q1: What is the maximal resolution ratio that DS90UB935 suport ?

Part Number: DS90UB935-Q1

Dear TI :

    What is the maximal resolution ratio that DS90UB935/936 suport ? If it can support 1920x1080/ 60Hz ? thanks!

  • Hello,

    This would depend on the number of bits per pixel of your imager.

    You can use the following equation to calculate your required forward channel rate: Horizontal res * vertical res * frame rate * #bits per pixel * 35% overhead. If the calculated forward channel rate is lower than 3Gbps, then 935/936 should work.

    If the calculated forward channel rate is greater than 3Gbps, you may need to consider higher data rate SerDes like the 953/954.

    Best,
    Jiashow