This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867IS: RGMII at 100M

Genius 17965 points

Part Number: DP83867IS

Hello,

 

I have a question about RGMII at 100Mbps mode.

Now I uses DP838367IS RGMII and it communicate in 100M mode.

When I monitored RGMII waveform during 100M communication, I found TXD was about 35nsec delayed to TX_CLK.

And there is no problem with this delay. It works well.

 

But DP83867IS RGMII specification says TskewR min is 1ns and max is 2.6ns.

From this specification, I don’t think 35nsec delay is acceptable. But it looks it is working.

So my question is that is required TskewR value at 100M mode different from 1G mode?

 

Regards,

Oba