Part Number: DS125DF410
Hi Team,
I have a question on Retimer IC DS125DF410 Signal Detect,
I would like to set Signal Detect to be turned on when a certain level or more of signal is input. Is the register that can change the signal level the following address?
Channel Register 0x14 bits4, 5
It seems that you can change to 4 levels with this 2-bit register,
How much will the input level be asserted for the following four combinations?
bit5 bit4
0 0 ← Is it 0V?
0 1
1 0
1 1
Also, do you think that the signal detect circuit does not start up if input of bit 2 and 3 of the same register is below a certain level?