Part Number: TPS65988
Hi Sir
I want to ask a experence question! I am working on a new project which might be 60W power needed.
Can I use internal power switch MOS to work 20V/3A power ? Would it make thermal issue on system or broken chip?
Do we have any test data or advice of this design?
The reason is that I want to replace CYPD5225(CCG5), and the cost need compare.
If we use internal power switch, then the total BOM cost will better then CYPD.
Thanks for feedback.
BR
Bruce