Part Number: TPS65987D
Other Parts Discussed in Thread: TIDA-050014, TIDA-050012
Hi,
We are using TPS65987D in our design and would like to connect 20V to a sink. A simplified diagram of our application is shown below.
It looks like from the following thread (scroll down till the end), it may be possible to do so.
However, the thread did not really mention how to set the source output to a voltage other than 5V by default. My question is:
How should I program the source and sink so that they automatically start the PD contract from 20V without having to start from 5V?
I have the .pjt files of TIDA-050012 and TIDA-050014 from the following links. Who knows modifying these files might be easier.
Regards,
Hermawan Mulyono