Part Number: TCA9800
Hi, Please look at TCA9800 datasheet Figure 18. In this usage the TCA9800 SDAB and SCLB pins drive the '9715 SDAA and SCLA pins via the internal current sources in the '9800 to generate a logic HI at the the '9517 pins. The designer must be certain that these current sources will pull up the '9517 SDAA and SCLA pins to a voltage that is at least the Vih MIN spec of the '9517, which is Vcca * 0.7V. I'm sure the '9800 meets this requirement; however, there is no spec in the '9800 datasheet that states it will. What is the MIN guaranteed Voh at 100uA (or some other reasonable load current) for the SDAB and SCLB pins of the TCA980x? Please add this to the datasheet for completeness. If I'm missing something and this information is already in the datasheet, please help me locate it.
Thanks, Andy