Hello,
i'm looking for a IC which is located on the "Client" (like a Phone, Tablet, ...) side of a USB QC wall adapter.
Does something like a USB-C Interface (Power Management) IC exist, which:
- can select the VBUS voltage via Quick Charge 2, 3 and 4 Interface (continuous mode)
- has a Microcontroller Interface like SPI or I2C
- optional: can monitor the VBUS voltage and or current
- optional: has a fixed 3.3V output for the Microcontroller