Part Number: TUSB9261
Hi,
I have build up an USB-SATA Interface with SPI flash of Mircochip: SST25VF512A . It will be flashed by the TI Windows Flash Burner tool. But the firmware doesn't start. The TUSB9261 is still in bootloader mode. Does it depend on the internal unchangeable bootloader software inside the TUSB9261 or depends it on the Firmware 1.05 or 1.06?
Br
Bjoern