Part Number: DS92LV010A
Other Parts Discussed in Thread: DS90LV019
Hi,
I need do translate LVDS to LVTTL/TTL logic level.
I only have 5V Vcc.
I fount the DS92LV010A (didn't find a single receiver - are they any?).
Is it safe to use it as a regular LVDS, with 100ohm input diff. termination, (and interface transmitter like the DS90LV011)?
by datasheet, it designet do work as part of a bidirectional bus, with diff. 27ohm termination.
(I also found the DS90LV019, but it's a 16-pin package for a single receiver..)
Thanks!
Max