Part Number: TCA4311A
Hello,
My customer has a question about TCA4311A.
[Q]
My customer is trying to connect as follows:
- SDAIN/SCLIN: card
- SDAOUT/SCLOUT: backplane
Because they use the card as a master for I2C communication, they think it is necessary to connect as such.
Is such a connection possible?
I think that the connection should be as described in D / S.
That's because that connection is necessary to support hot-swap.
And I think that the card side can be used as a master for I2C communication even if it is a D / S connection.
Is my understanding correct?
Best Regards,
Kaede Kudo