Part Number: SN65HVD888
HI,
As per SN65HVD888DR datasheet Application Information mentioned RL DIFFERENTIAL TERMINATION for 54 Ω.
For 120Ω.RL DIFFERENTIAL TERMINATION suggest suitable RFS PULLUP / RFS PULLDOWN resistor value.
Thanks
Rajan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65HVD888
HI,
As per SN65HVD888DR datasheet Application Information mentioned RL DIFFERENTIAL TERMINATION for 54 Ω.
For 120Ω.RL DIFFERENTIAL TERMINATION suggest suitable RFS PULLUP / RFS PULLDOWN resistor value.
Thanks
Rajan
Rajan,
The 54Ohm termination takes all load into account. For example, assume you have two 120Ohm termination at both ends of communication. With some nodes attached to the bus (RX input resistance), the equivalent resistance becomes 54Ohm.
If you want to have a fail-safe bias on the bus, you can refer to this app note for the details. The basic idea is to create a 120Ohm with the termination and 2 RSF, while the bus voltage is biased around 200mV to 250mV in idle.
Please let me know if you have more questions.
Regards,
Hao
Hi Hao,
Thank you for your support,
As per SN65HVD888 datasheet Electrical Characteristics VOH Receiver high-level output voltage MIN = 2.4V and TYP = VCC – 0.3 for IOH = –8 mA.
I can't able to see the different IOH current with respect to VOH graph image.
So please let us know for 2 and 4mA IOH current respective VOH MIN value.
Thanks
Rajan