This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello!
I have a problem need to be solved, about the DS90CF384 used to driver a TFT LCD with 320x152 pixe (RGB888). but the LVDS CLK of DS90CF384 is look like out over the range from 20 to 65MHz. dou you have any advise to me? We can we use DS90CF384 to drive the LCD(320*152 pixe) with RGB(24bit)?